SAFEPARAM.IOFAILUREACKSOURCE

Description

Indicates which safe input, if any, is configured as the I/O Failure acknowledge source. This parameter is configured using FSoE or WorkBench . When configured, it allows clearing of an I/O Failure warning (W9011) using the configured safety input.

WorkBench Parameters Editor Common > General with the I/O Failure Acknowledgement option set

Versions

Action

Version

Notes

Implemented

02-01-02-000

General Information

Type

Read/Write

Units

N/A

Range

0...4

Default Value

0 (No safe input)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

SAFEPARAM.IOFAILUREACKSOURCE

3100h

01h

Unsigned8

-

-

Read/Write

No